Part Number: RM44L520
Other Parts Discussed in Thread: HALCOGEN,
Hello all,
I have a board I am developing firmware for and one of the LEDs is connected to pin 58, which seems to be configured for use as the ADC1 Event pin. The data sheet says this pin can also be configured as GPIO, but when going into Halcogen, there doesn't seem to be any option to configure this pin for use as GPIO. I was wondering if there is some setting I am missing in Halcogen to properly configure this pin for GPIO or if this is something I need to do manually within code composer studio. I'm happy to provide any additional information if what I have posted here isn't sufficient.
Thanks in advance for your help