Part Number: MSP432E411Y
Hello Everyone,
Could I please be provided both the "adc.c" and "timer.c" source files for the MSP432E411Y microcontroller? I have used the following link to source the header files for the aforementioned source files, however, there is no indication that the source files themselves are available.
The functions included inside of "adc.c" and "timer.c" in the above link are the versions I require.
I have also tried making a new project and seeing if the files are included with the driverlib, but they are not. Additionally, I have also tried downloading whole projects from the following link with no luck either:
https://dev.ti.com/tirex/explore/node?node=AJDS8Vpx6RDwlNjGgAiVqg__J4.hfJy__LATEST
I would really appreciate if I could be either provided the files or pointed to the right location to source them..
Regards,
Joseph