Part Number: EK-TM4C123GXL
Using the code below, the clock is set for 80 MHz. Here are some results for the interrrupt interval for various values in MAP_TimerLoadSet(). Have I setup something wrong?
Load Measured Expected
320 249.25 KHz 250 KHz
160 497 KHz 500 KHz
80 823 KHz 1 MHz
40 821 KHz 2 MHz
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#define SYSTEM_TICKS_PER_SECOND 1000000UL
volatile static uint64_t ticks;
void Timer0IntHandler();
uint64_t getTicks();
void
Timer0IntHandler()
{
static bool toggle = 1;
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
ticks++; // Microseconds since power up.
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2); //Blue
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0);
toggle = !toggle;
//Tickle scheduler...
}
int
main(void)
{
volatile uint32_t loops = 0;
volatile uint64_t t;
MAP_SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
// LED debugging setup
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2 | GPIO_PIN_3);
//Timer 0 setup.
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
MAP_IntMasterEnable();
MAP_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
MAP_TimerLoadSet(TIMER0_BASE, TIMER_A, 40UL); //(SysCtlClockGet() / SYSTEM_TICKS_PER_SECOND));
MAP_IntEnable(INT_TIMER0A);
MAP_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
MAP_TimerEnable(TIMER0_BASE, TIMER_A);
while(1)
{
}
}