Other Parts Discussed in Thread: AM3352
When I use the I2C external touch screen of am3352, when the touch screen touches multiple points, the I2C bus will die, and it will also cause the crash of am3352 and system reset.
What causes the CPU reset problem.
Look forward to your reply,Thanks.
The following is the error message,When the problem occurs, other devices on the I2C bus cannot communicate normally.
[ 62.805943] omap_i2c 44e0b000.i2c: controller timed out
[ 63.855660] atmel_mxt_ts 0-004b: __mxt_read_reg: i2c transfer failed (-110)
[ 63.863124] atmel_mxt_ts 0-004b: Failed to read 1 messages (-110)
[ 63.869572] atmel_mxt_ts 0-004b: Read: message failed (-110)
[ 64.894896] atmel_mxt_ts 0-004b: __mxt_read_reg: i2c transfer failed (-16)
[ 64.902006] atmel_mxt_ts 0-004b: Failed to read T44/T144 and T5 (-16)