Part Number: TMDSEMU110-U
Hello,
We ordered a XDS110 Debug Probe and it looks like it does not enumerate when connected to the USB port on my Windows 10 desktop computer. I checked device manager and it does not show up when plugged in. I also noticed neither D1 or D2 debugger LEDs light when plugged in. I checked the XDS110 instructions in the CSS product page and it states "Plug in the XDS110. It should be properly recognized by the system". I am unsure if there is something else I need to do, or if I have a hardware issue with this debugger. My setup is:
OS: Windows 10
CSS Version: 11.1.0.00011
Debug Probe: TMDSEMU110-U