Part Number: AM2432
Hi Team,
One of my customers has a few questions about GPMC-related clock. I've pasted their questions as below:
- Could you show timing constraints between GPMC_FCLK_MUX and other GPMC_* signals? On the datasheet, timing constraints between GPMC_FCLK and other GPMC_* signals are shown.
We have to use GPMC_FCLK_MUX because the slave device needs continuous bus clock. So We need timing constraints on GPMC_CLK_FMUX. - It seems that peripheral blocks need both *_FCLK and *_ICLK. (for example p7326 Figure 12-1589. GPMC Integration)
There is a little information on *_ICLK signal. We know only 1)it is described as Interface clock, 2)it is generated from MAIN_SYSCLK0 of PLL_CTRL0 and divided by 2.
What should we do about setting *_ICLK from software? (frequency setting? which divider block should we use?) - Are the signals named GPMC_* and signals named GPMC0_* are identical? In both the datasheet and the TRM, Two notations are mixed.
- About the clock source selection of GPMC_FCLK. it is mentioned on Table 5-613(page 2418) and Figure 12-1589(page7326). but it seems that Table5-613 and Figure12-1589 say different information.
Best regards,
Mari Tsunoda