Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: TCAN1042H
I copied the example C:\ti\TivaWare_C_Series-2.2.0.295\examples\peripherals\can\simple_tx.c and built it. The code runs but I got no wiggles out of PB5, it just stays high. PB4 and 5 are RX and TX, not CANL and CANH so I did not think I needed terminators. Also In applications I have seen it often feeds a device like a TCAN1042H that converts tx and rx into/from CANH/CANL. What the heck, I put 130 ohms between them and started seeing signals for a few seconds and then it would shut down.
Also the polarity of RX is the same as TX, where before it was always low. I ain't the sharpest knife in the drawer and this is a whole new can of worms for me so a bit of explanation would help. When my prototype arrives the TM123 will be connected to a TCAN1042H.
Thanks,
John