Part Number: AM2432
Hi Team,
My customer has a question about adding source code files. They eventually plan on not using CCS to build, but to use makefiles.
Should they edit the makefile and add the source code file or should they add the source code file in CCS first, and then build using the makefile generated via CCS?
They saw in the makefile that it says that the makefile should not be edited. Furthermore, they also saw on E2E that using the makefile generated from building in CCS is recommended, and that questions regarding any makefiles edited/made by users are not supported. Therefore, is the CCS method the only recommendation and should users not generate/edit their own makefiles? Is there a reason for this?
Best regards,
Mari Tsunoda