Part Number: TMS570LC4357
I have created a project with below tasks and tested the periodicity of each task which was as expected, but when I changed the stack size of the tasks as shown in second part I observed task is not executing with fixed period.
Can you please let me know the exact root cause of the behavior and its solution.
#if 0
/* all task executes with configured period*/
xTaskCreate(vEv_20ms1,"Test_20ms1", 1000, NULL, 23, NULL);
xTaskCreate(vEv_50ms1,"Test_50ms1", 100, NULL, 28, NULL);
xTaskCreate(vEv_50ms2,"Test_50ms2", 100, NULL, 25, NULL);
xTaskCreate(vEv_100ms1,"Test_100ms1", 100, NULL, 1, NULL);
xTaskCreate(vEv_100ms2,"Test_100ms2", 100, NULL, 1, NULL);
xTaskCreate(vEv_100ms3,"Test_100ms3", 100, NULL, 1, NULL);
xTaskCreate(vEv_100ms4,"Test_100ms4", 100, NULL, 1, NULL);
xTaskCreate(vEv_100ms5,"Test_100ms5", 100, NULL, 1, NULL);
xTaskCreate(vEv_100ms6,"Test_100ms6", 100, NULL, 1, NULL);
xTaskCreate(vEv_500ms1,"Test_500ms1", 100, NULL, 1, NULL);
xTaskCreate(vEv_500ms2,"Test_500ms2", 100, NULL, 1, NULL);
xTaskCreate(vEv_500ms3,"Test_500ms3", 100, NULL, 1, NULL);
xTaskCreate(vEv_500ms4,"Test_500ms4", 100, NULL, 1, NULL);
xTaskCreate(vEv_1000ms1,"Test_1000ms1", 100, NULL, 1, NULL);
xTaskCreate(vEv_1000ms2,"Test_1000ms2", 100, NULL, 1, NULL);
#else
/* Task lost its periodicity*/
xTaskCreate(vEv_20ms1,"Test_20ms1", 4000, NULL, 23, NULL);
xTaskCreate(vEv_50ms1,"Test_50ms1", 200, NULL, 27, NULL);
xTaskCreate(vEv_50ms2,"Test_50ms2", 500, NULL, 25, NULL);
xTaskCreate(vEv_100ms1,"Test_100ms1", 1000, NULL, 21, NULL);
xTaskCreate(vEv_100ms2,"Test_100ms2", 1000, NULL, 18, NULL);
xTaskCreate(vEv_100ms3,"Test_100ms3", 200, NULL, 17, NULL);
xTaskCreate(vEv_100ms4,"Test_100ms4", 4000, NULL, 16, NULL);
xTaskCreate(vEv_100ms5,"Test_100ms5", 500, NULL, 15, NULL);
xTaskCreate(vEv_100ms6,"Test_100ms6", 1000, NULL, 14, NULL);
xTaskCreate(vEv_500ms1,"Test_500ms1", 500, NULL, 12, NULL);
xTaskCreate(vEv_500ms2,"Test_500ms2", 400, NULL, 10, NULL);
xTaskCreate(vEv_500ms3,"Test_500ms3", 400, NULL, 8, NULL);
xTaskCreate(vEv_500ms4,"Test_500ms4", 1000, NULL, 6, NULL);
xTaskCreate(vEv_1000ms1,"Test_1000ms1", 1000, NULL, 4, NULL);
xTaskCreate(vEv_1000ms2,"Test_1000ms2", 500, NULL, 2, NULL);
#endif
FYI
FreeRTOSConfig.h is as below
#define configUSE_PREEMPTION 1
#define configUSE_PORT_OPTIMISED_TASK_SELECTION 1
#define configUSE_FPU 1
#define configUSE_IDLE_HOOK 0
#define configUSE_TICK_HOOK 0
#define configUSE_TRACE_FACILITY 1
#define configUSE_16_BIT_TICKS 0
#define configCPU_CLOCK_HZ ( ( unsigned portLONG ) 80000000 ) /* Timer clock. */
#define configTICK_RATE_HZ ( ( TickType_t ) 1000 )
#define configMAX_PRIORITIES ( 30 )
#define configMINIMAL_STACK_SIZE ( ( unsigned portSHORT ) 128 )
#define configTOTAL_HEAP_SIZE ( ( size_t ) 250000 )
#define configMAX_TASK_NAME_LEN ( 16 )
#define configIDLE_SHOULD_YIELD 1
#define configGENERATE_RUN_TIME_STATS 1
#define configUSE_MALLOC_FAILED_HOOK 0
Case 1: Working version maximum task almost with same stack and priority
Result: Works normally
Case 2: Changed stack and priority
Result: Works with abnormal period
Case3: Changed only stack size with respect to working version
Result: Get stuck at b dataEntry
Case4: Changed only priority with respect to working version
Result: executes with expected period, normal behaviour
If its due to data exception, can you please guide me how to fix it? Its debug procedure.
heap configured is more than the total stack configured by all task and there is no function in any task so stack usage is might be around 20 30 bytes.
Thanks and Regards,
Kishor