Part Number: AM2634
Hi experts,
could you please share the total power consumption data on each power-supply pin? I can find power consumption data for some analog IPs and PWM from datasheet chapter 7.7, but please also provide a total number just like chapter 7.6.
Another question is that my customer found the current consumption of 1.2VDD will increase from 0.2A to 0.7A when connecting the target via debugger. The reason is the R5F's clock, right? The default clk source for R5F is WUCPUCLK 25MHz, and after using GEL file to connect the target, the clk of R5F core will be 400 MHz. I want to double confirm if the 0.7A is acceptable?
Best Regards,
Will