Part Number: MSP432E411Y
Hello,
I integrated the mqttclient_MSP_EXP432E401Y_tirtos_ccs and httpserver_MSP_EXP432E401Y_tirtos_ccs from the SimpleLink MSP432E4 SDK (4.20.00.12) TI-RTOS-examples into the firmware for our MSP432E411Y-Controller. It is connected to a router with DHCP-server which is connected to a computer with a browser and a Mosquitto running.
This works fine, until I connect the xds100 debug-probe and start the debug-mode of the code composer studio (11.1.0.00011). If I dis- and reconnect the network-cable from the computer or the computer goes into energy saving mode, the controller restarts due to a watchdog timeout and the debugger gets disconnected. This does not happen with the ccs in editor-mode.
Is there something that takes so much longer in debug mode during network connection? What can I do to avoid this?
Thank You,
Boris