Part Number: AM2432
Hello,
In reference to the TMDS243GPEVM schematic I noticed that the DDR4 VTT supply enable (DDR_VTT_EN) is connected to an OSPI chip select (L18, OSPI0_CSN1). For our design, it made more sense to connect the DDR4 VTT supply enable to a GPIO pin because it can drive 3.3V instead of the OSPI CS 1.8V. However, I am unsure if the GPIO pin mux can be set and toggled during boot, before the application is loaded and run from DDR4. I just need to make sure my firmware team will be able to enable the DDR4 VTT supply with a GPIO, before DDR4 is used.
If the TMDS243GPEVM design has the OSPI CS pin mux set to a GPIO to toggle the DDR4 VTT supply enable, that would probably answer my question.
Thanks,
Tom