Other Parts Discussed in Thread: LM3S2110
Dear Sir,
I design a evaluation board using LM3S9B92IQC80C3, which is almost the same as ek-lm3s9b92. The minor difference is that PB4, PB5 are used as CAN pins. When I debug the can_fifo example, the routine can not enter into the CANIntHandler(), I cannot find the reason.
By the way, the routine of can_device_fifo has been running in the CAN device evaluation board based on LM3S2110IQC25A2.
Then, I load the program into IDM_SBC_RDK(LM3S9B92IQC80B1), and the routine can enter into the CANIntHandler(), but stopped waiting for all bytes go out for ever. The the circuits for the CAN node are the same, why the results are different?
Is there any program fit for LM3S9B92 How Can I make the CAN controller of a LM3S9B92IQC80C3 work correctly ?
The can_fifo and can_device_fifo files are as follows:
6232.can_device_fifo(lm3s2110).rar
Any suggestions will be appreciated!
Regards,
Michael Lee.