Part Number: SM470R1B1M-HT
Hi team,
Here's an issue from the customer may need your help:
For the same project, the compiler has two conflicting resolutions for the same bit-domain structure, as shown in the following code examples:
1) Bit domain structure definition:
typedef volatile struct
{
UBYTE rsv_ccr[3];
union
{
UBYTE ccr_UB;
struct
{
UBYTE CharLength_B3 : 3;//bit0~bit2
UBYTE Mode_B1 : 1;//bit3
UBYTE Async_B1 : 1;
UBYTE ParityEN_B1 : 1;
UBYTE Parity_B1 : 1;
UBYTE Stop_B1 : 1;//bit7
} ccr_ST;
} ccr_UN;
。。。
} SCI_ST;
Defines a pointer to type SCI_ST: SCI_ST * Sci_PST = &SCI1;
2) The main function has a C operating instruction
Sci_PST->ccr_UN.ccr_ST.CharLength_B3 = 7;
3) The initialization function has a C operating instruction
Sci_PST->ccr_UN.ccr_ST.CharLength_B3 = 7;
4) The result compiled within the main function and the initialization function is conflicting
Within the main function:

With the initialize function:

5) Conflicting: The main function assumes that the bit field member "CharLength_B3" is placed in the lower 3 bits. The initialization function assumes that the bit field member "CharLength_B3" is placed in the upper 3 bits.
Why is that?
Could you help check this case? Thanks.
Best Regards,
Cherry