Part Number: AM2432
Hi Team,
I received two questions from my customer regarding pin assignment as follows.
- According to 6.4 Pin Connectivity Requirements on AM243x datasheet, I2C0_SCL, I2C0_SDA, MCU_I2C0_SCL, MCU_U2C0_SDA pins need to be pulled-up externally. Are external pull-ups necessary even if we don't use these pins for I2C function? We use the B18pin(I2C0_SDA) for GPIO0_65, and other pins are not used. So we want them to be Un-connected.
- Why are internal pull-ups not available on I2C0_SCL, I2C0_SDA, MCU_I2C0_SCL, MCU_U2C0_SDA?
According to 6.4 Pin Connectivity Requirements on AM243x datasheet, "Each of these balls must be connected to the corresponding power supply(1) through separate external pull resistors to ensure these balls are held to a valid logic high level."
Any insight is very much appreciated.
Best regards,
Mari Tsunoda