Other Parts Discussed in Thread: AM2634
Hello,
I need additional information about the AM2634 Q1 / SPRSP74 - MARCH 2022.
In the datasheet CLKOUT0 (Ball M2) and CLKOUT1 (Ball B16) are mentioned.
I would like to feed these CLKOUTx into an external FPGA. Ideally, the AM2634 and the FPGA would have a syncronized clock.
Where can I find the characteristics of these CLKOUTx pins?
How much capacitance and mA can these pins drive?
I plan to use a 25MMz or 50MHz oscillator on EXT_REFCLK0 (Ball P2).
Is it possible to drive the AM2364 with a 50MHz clock, or do I need to use 25MHz?
What can I expect in terms of jitter at CLKOUT0 and CLKOUT1 if the clock is derived from EXT_REFCLK0 / 50MHz or 25MHz / 100ppm?
br,
Bernhard