This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2431: Octal SPI using a PSRAM device and wanting to use Execute in Place (XIP)

Part Number: AM2431

I am considering using an Octal SPI memory PSRAM device like the AP Memory  APS6408L-3OBMX-BA

I wanted to be able to run Execute in Place (XIP) with the RAM device.

I know the AM2431 supports XIP on the Octal SPI interface, but since I am using a PSRAM device this is not specifically stated that it would support it and there are no specific mention in the PSRAM supporting XIP. What I am wondering is if TI has ever tried this or has any comments on this topology