Part Number: MSP-EXP432E401Y
Other Parts Discussed in Thread: MSP432E401Y
Can I use the USB port that is connected directly to the MSP432E401Y on the MSP-EXP432E401Y development board to be a serial port? If so, I have a couple of questions:
1. It looks like the USB port is connected to PL6 and PL7. Is it possible to just configure these pins to be Tx and Rx of one of the UARTS? Any information on how to do that would be very helpful.
2. I'd like to set the baud rate to be 38400 and it would be very helpful if I knew which values for UARTIBRD and UARTFBRD I should use. Or, I could calculate them myself if I knew the value for the system clock for the board.
Thank you.