We are considering having two devices on the OSPI interface.
One of the devices would be an OSPI NOR flash part that has DQS support.
If I connect the DQS signal between the TI part and the OSPI NOR flash part and then also have a 2nd QSPI part on a different CS, would that be an acceptable configuration.
The reason I ask is in the cases were I am using the QSPI part wouldn't the DQS signal be inactive. If that is the case would that cause an issue in the read timing for the TI part?