This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310F128 UART BSP documentation request

Hi,

We are using the mentioned processor CC1310F128, and struggeling with the documentation of the UART Module.

I need the following information:

1: unit of UART_Params_.readTimeout and UART_Params_.writeTimeout

2: When I use the Blocking mode, when is the UART_Params_.readTimeout applied?

3: What happens when I call UART_read() in blocking mode and not directly a byte is received. Is than the UART_Params_.readTimeout applied?

4: What happens when a gap happens for example I call UART_read(handle, buffer, 10) and after 5 bytes a little delay happens. Is than the UART_Params_.readTimeout applied or is there the 32Bit timeout applied

5: In non blocking mode, is there a timeout applied? In the code comments it says, that UART_Params_.readTimeout is just for blocking operation.

Kind Regards

Christian