Part Number: TM4C129XNCZAD
Hello Everyone,
I am trying to use external SDRAM (W9812G6KH-6) with TM4C129X microcontroller so that I can drive LCD module with bigger frame buffer size.
I have written the following EPI code for External SDRAM. I am using PH0,PH1,PH2,PH3,PN2,PN3 pins.
#define EPI_PORTA_PINS (GPIO_PIN_7 | GPIO_PIN_6)
#define EPI_PORTB_PINS (GPIO_PIN_3)
#define EPI_PORTC_PINS (GPIO_PIN_7 | GPIO_PIN_6 | GPIO_PIN_5 | GPIO_PIN_4)
#define EPI_PORTG_PINS (GPIO_PIN_1 | GPIO_PIN_0)
#define EPI_PORTH_PINS (GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 |GPIO_PIN_0)
#define EPI_PORTK_PINS (GPIO_PIN_5 )
#define EPI_PORTL_PINS (GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0)
#define EPI_PORTM_PINS (GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0)
#define EPI_PORTN_PINS (GPIO_PIN_3 | GPIO_PIN_2)
static volatile uint16_t *g_pui16EPISdram,p11,p22,p33,p44;
void EPI_INIT(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_EPI0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
GPIO_PORTA_AHB_PCTL_R |= 0xFF000000;
GPIO_PORTB_AHB_PCTL_R |= 0x0000F000;
GPIO_PORTC_AHB_PCTL_R |= 0xFFFF0000;
GPIO_PORTG_AHB_PCTL_R |= 0x000000FF;
GPIO_PORTH_AHB_PCTL_R |= 0x0000FFFF;
GPIO_PORTK_PCTL_R |= 0x00F00000;
GPIO_PORTL_PCTL_R |= 0x0000FFFF;
GPIO_PORTM_PCTL_R |= 0x0000FFFF;
GPIO_PORTN_PCTL_R |= 0x0000FF00;
GPIOPinTypeEPI(GPIO_PORTA_BASE, EPI_PORTA_PINS);
GPIOPinTypeEPI(GPIO_PORTB_BASE, EPI_PORTB_PINS);
GPIOPinTypeEPI(GPIO_PORTC_BASE, EPI_PORTC_PINS);
GPIOPinTypeEPI(GPIO_PORTG_BASE, EPI_PORTG_PINS);
GPIOPinTypeEPI(GPIO_PORTH_BASE, EPI_PORTH_PINS);
GPIOPinTypeEPI(GPIO_PORTK_BASE, EPI_PORTK_PINS);
GPIOPinTypeEPI(GPIO_PORTL_BASE, EPI_PORTL_PINS);
GPIOPinTypeEPI(GPIO_PORTM_BASE, EPI_PORTM_PINS);
GPIOPinTypeEPI(GPIO_PORTN_BASE, EPI_PORTN_PINS);
EPIDividerSet(EPI0_BASE, 1);
EPIModeSet(EPI0_BASE, EPI_MODE_SDRAM);
EPIConfigSDRAMSet(EPI0_BASE, (EPI_SDRAM_CORE_FREQ_50_100 | EPI_SDRAM_FULL_POWER |EPI_SDRAM_SIZE_128MBIT), 1024);
EPIAddressMapSet(EPI0_BASE, EPI_ADDR_RAM_SIZE_16MB | EPI_ADDR_RAM_BASE_6);
while(HWREG(EPI0_BASE + EPI_O_STAT) & EPI_STAT_INITSEQ)
{
}
g_pui16EPISdram = (uint16_t *)0x60000000;
g_pui16EPISdram[0] = 0x21;
g_pui16EPISdram[1] = 0x124;
g_pui16EPISdram[2] = 0x213;
g_pui16EPISdram[3] = 0x123;
p11 = g_pui16EPISdram[0];
p22 = g_pui16EPISdram[1];
p33 = g_pui16EPISdram[2];
p44 = g_pui16EPISdram[3];
}
int main(void)
{
MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |SYSCTL_OSC_MAIN |SYSCTL_USE_PLL |SYSCTL_CFG_VCO_240), 120000000);
EPI_INIT();
while(1){}
}
When I'm running the code, I am getting p11=0,p22=1,p33=2,p44=3.
I am to know what's wrong with my code?