Part Number: TM4C123GH6PM
Hi team,
The stack size is described in the cmd file as "__STACK_TOP = __stack + 1024;".
However, when I checked the MAP file, I found the following
Add:0x20000928 = __stack
Add:0x20000d28 = __STACK_END
Add:0x20000d28 = __STACK_TOP
Why are the address values of __STACK_END and __STACK_TOP the same?
Also, if I want to change the addresses of __STACK_END and __STACK_TOP, what kind of operation should I do?
The version of CCS I was using is (Ver:11.1.0.00011)
Sincerely.
Ryu