Part Number: TMS570LC4357
I havethe SPNA190 (UART Bootloader) code. There is no directory for the 570LC4357 however. Which flavor should I start with and should it run without modifications?
Regards,
Mark Samarin
Afuzion, Inc.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
I havethe SPNA190 (UART Bootloader) code. There is no directory for the 570LC4357 however. Which flavor should I start with and should it run without modifications?
Regards,
Mark Samarin
Afuzion, Inc.
Also:
1) The only F021 API libraries available appear to be for R4 cores only. Will these run OK on the R5F cores? Which one should I use with the 570LC4357 and FP enabled?
2) When I try to include F021_API_CortexR4_BE_L2FMC_V3D16.lib in my IAR project I get the following link Errors:
Linking
Error[Li005]: no definition for "__iar_system_Mtxinit" [referenced from xsyslock_mtx.o(dl7Sx_tbn.a)]
Error[Li005]: no definition for "__iar_system_Mtxlock" [referenced from xsyslock_mtx.o(dl7Sx_tbn.a)]
Error[Li005]: no definition for "__iar_system_Mtxdst" [referenced from xsyslock_mtx.o(dl7Sx_tbn.a)]
Error while running Linker
Thank you for this. We will not be able to use the F021 Library as this is a DO-178B project and we have to qualify our source code. Is is possible to get the source code for the LC43x version of this? It would help greatly.
Regards,
Mark Samarin
Afuzion, Inc
Is is possible to get the source code for the LC43x version of this?
TMS570LS1224: F021 Flash API validation has some information about that.
I don't know what the process is to obtain the source code under a signed license agreement with TI.