Part Number: RM57L843
Hi,
My customer is developing with the RM57L843.
He requires the information for the Euromap 67.
Can I get some information about the Euromap 67 Interface with the RM57L843 or other MCUs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Euromap 67 is just a connection between the injection moulding machine and the handling device/robot. You can implement this interface on your PCB board. The Plug on the handling device looks like:

RM57L843 is a high-performance ARM Cortex-R-based MCU. The RM57L843 device has on-chip diagnostic features including: dual CPUs in lockstep, Built-In Self-Test (BIST) logic for CPU, the N2HET coprocessors, and for on-chip SRAMs; ECC protection on the L1 caches, L2 flash, and SRAM memories. The device also supports ECC or parity protection on peripheral memories and loopback capability on peripheral I/Os. The RM57L843 device integrates two ARM Cortex-R5F floating-point CPUs, operating in lockstep, which can run up to 330 MHz.
With integrated safety features and a wide choice of communication and control peripherals, the RM57L843 device is an ideal solution for high-performance real-time control applications with safety critical requirements.