This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: DMA ECC test fails randomly

Part Number: TMS570LC4357

Hi,

We implemented DMA ECC test as per Hercules\SafeTI Diagnostic Library file. It works fine but observed it fails randomly. 

dmaBadECC address is set to 0xFFF80010u and expected same address in ram1erraddr when read the DMA ECC SIngle-Bit Error Address Register

(DMAECCSBE) after triggering single bit or double bit error. But sometimes it returns 0xFFF8001Cu address instead of 0xFFF80010u. As error occurs randomly, not able to debug.

Could you please advice what could be the problem or how to re-produce it constantly to debug further.