Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hi all:
How to disable MPU function? such as write 0 to some registers?
Best Wish
Li
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hi all:
How to disable MPU function? such as write 0 to some registers?
Best Wish
Li
what's the base address of MPU register?
The MPU registers are not memory mapped. They are read and written through MRC and MRC instructions, for example:
MRC p15, 0, R1, c1, c0, 0 ; read CP15 register 1
ORR R1, R1, #0x1
DSB
MCR p15, 0, R1, c1, c0, 0 ; enable MPU
How to disable MPU function?
The following code is an example of disabling the MPU:
MRC p15, 0, R1, c1, c0, 0 ; read CP15 register 1
BIC R1, R1, #0x1
DSB
MCR p15, 0, R1, c1, c0, 0 ; disable MPU
ISB
The HALCoGen generates code to configure MPU, enable MPU, or disable MPU:
_mpuInit_();
_mpuEnable_();
_mpuDisable_();
You can use c code to call the ARM instructions.
asm(" MRC p15, 0, R1, c1, c0, 0"); //read CP15 register 1
asm(" BIC R1, R1, #0x1");
asm(" DSB");
asm(" MCR p15, 0, R1, c1, c0, 0); //disable MPU
asm(" ISB");
as I said that you can call "_mpuDisable_();" to disable the MPU.