Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: EK-TM4C123GXL, LMFLASHPROGRAMMER
Hi, I've been using using EK-TM4C1294XL to load firmware into an external board for a while and now I getting "Error connecting to the target", I had some earth problems recently and I think U20(tm4c123gh6pmi7) may be damaged. I'm connecting EK-TM4C1294XL trough USB connector U22 and already removed R6,R7,R8,R10,R11,R15,R16.
How can I check if U20 is damaged, I measure with osciloscope in jtag pins while trying to program (Error connecting to the target) from code composer studio and I see no switching in the signals, also without the target connected I measure voltage on jtag pins: reset=3.3V, TDO=0.75V, TDI=3.11V, TMS=0.75V and TCK=0.75V.
if U20 is damaged, is possible to replace the part? I have some tm4c123gh6pmi7.
thanks
Rafael