This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: Is QSPI XIP Supported

Part Number: AM2634

Hello TI Experts,

Would you be able to confirm the ability of the TI AM2634 microcontroller to use eXecute In Place (XIP) through the QSPI memory interface?

The current state of MCU-PLUS_SDK_AM263X (08.02.00.28) documentation does not include any examples of this behavior that I am able to find. I was expecting to find the section "AM263x MCU+ SDK: Enabling XIP or eXecute In Place", similar to what is currently available in the AM24x SDK.

The EXT_FLASH0 and EXT_FLASH1 sections detailed in the TRM memory map (Table 2-1), the build chain tools, and the default linker file all indicate this functionality should eventually be present. If this is in fact a supported behavior like I am led to believe, is there an expected delivery date based on the internal development schedule for an example?

Thanks,

Steven