Part Number: MSP-EXP432E401Y
Other Parts Discussed in Thread: MSP432E401Y
I'm trying to re-create this development board on a prototype board of our application so I can use all the debug features while I design the interface to the peripherals the MSP432E401Y is going to be connected to.
Everything is pretty straight forward except for the layout near the USB port on the XDS110 section of this development board. There is a mysterious 8 pin IC near the connector that I can't find any information on. The schematic for this section is on page 27 of SLAU748B (SimpleLink Ethernet MSP432E401Y Microcontroller LaunchPad Development KIT), but neither the mysterious 8 pin IC or the USB connector are included on that schematic.
Can anyone tell me where I might find the schematic for this section that includes the 8 pin IC and the USB connector so I can finish designing it onto my prototype board?
Thank you.