Hi TI Experts,
after implementing the changes from the thread AM2432: Emac mode SWTICH is not working in SDK the example we get the following errors while trying to start the system.
ICSSG Switch Test
Icssg_ioctlPortLinkCfg: icssg1: Port 1: failed to set acceptable frame check: -3
Icssg_ioctlInternal: icssg1: Port 1: failed to open port link: -3
Icssg_ioctl: icssg1: failed to run ICSSG Per IOCTL 0x01000102: -3
EnetPer_ioctl: icssg1: Failed to do IOCTL cmd 0x01000102: -3
Enet_ioctl: icssg1: IOCTL 0x01000102 failed: -3
EnetMcm_enablePorts() failed to open MAC port: -3
Icssg_ioctlPortLinkCfg: icssg1: Port 2: failed to set acceptable frame check: -3
Icssg_ioctlInternal: icssg1: Port 2: failed to open port link: -3
Icssg_ioctl: icssg1: failed to run ICSSG Per IOCTL 0x01000102: -3
EnetPer_ioctl: icssg1: Failed to do IOCTL cmd 0x01000102: -3
Enet_ioctl: icssg1: IOCTL 0x01000102 failed: -3
EnetMcm_enablePorts() failed to open MAC port: -3
EnetMcm_enablePorts failed
Assertion @ Line: 929 in C:/tfs/FeldbusGenC/dev/dev_PnLight/Source/Platform/Extern/am243x/v1/source/networking/enet/utils/V3/enet_mcm.c: ENET_SOK == status : failed !!!
Did we miss anything?
Kind regards,
Sven