Part Number: LP-AM243
Hello TI-Support Team,
I have got some questions about the SBL_x, especially SBL_null.
Due to the descriptions for the examples, the "Flash SOC Initialization Binary" with downloading of SBL_null into flash shall be done once before going on with the examples.
1. What is it really for ? Is it a prerequisite for debugging SW via JTAG interface ?
2. It shall be done once because there is no access to MCU via JTAG interface possible ?
3. Access to MCU via JTAG is there any prerequisites ?
I would like to understand it clearly since on our target hardware there will be NO any serial interfaces, the boot mode will be set fixed to OSPI/QSPI Flash via resistors, only the JTAG interface will be provided. So there is only one way to download the SBL into the flash => via JTAG interface.
Thanks in advance for your reply and clarification.