Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: SEGGER
Hello,
I have a few questions regarding the programmimg of the device in circuit. I was hoping someone could point me to the right docs.
1. how to create the 'release version' of the code developed on a development board
2. how to actually program it into the device
- is it as straight forward as bringing the 4 JTAG pins out on the target board using a connector or bed of nails,
- then use a programmer like segger or lm flash that can write the release code (*.out ??) into the device using the JTAG interface?
- does the board need to powered or is the JTAG enough.
Thank You
P