Other Parts Discussed in Thread: RM44L920, HALCOGEN
Hello,
I am using the pwm generation on the RM44L920 platform using the HET module. I use the code generated by HAlcogen version 04.07.01.
The pwm generation works if the duty cycle is between 1%-100%. However if the duty cycle was set before to 100% by calling pwmSetDuty(), setting the duty cycle to 0% does not force the output pin low. The ouput pin keeps high.
Is this a known issue of HET that changing of duty cycle from 100% to 0% doesn't work?
Thanks an regards
Chunyan