Part Number: EK-TM4C123GXL
Hi Team,
The system cannot work when changing a system clock setting

Best Regards
James Man
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EK-TM4C123GXL
Hi Team,
The system cannot work when changing a system clock setting

Best Regards
James Man
Hello Depeng,
The images you tried to post did not load correctly.
Also if this is specifically about the EK-TM4C123GXL - neither of those should work because the board is populated with a 16MHz crystal so you need to make sure the SYSCTL_XTAL parameter reflects that:
//
// Set the system clock to run from the PLL at 80MHz.
//
SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_INT |
SYSCTL_XTAL_16MHZ);
That runs from the PLL.
//
// Set the clocking to run directly from the crystal.
//
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
This alternatively runs from the crystal itself.
Best Regards,
Ralph Jacobi