Part Number: TMS570LC4357
I'm working on accessing FEE of TMS570LC4357. To ensure the integrity of read data, I want to know the ECC Error Status (No error/1-bit error/2-bit error). Is there any function which returns this status?
Please help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
I'm working on accessing FEE of TMS570LC4357. To ensure the integrity of read data, I want to know the ECC Error Status (No error/1-bit error/2-bit error). Is there any function which returns this status?
Please help.
Hi Harshal,
The on-chip FEE memory is supported by SECDED ECC diagnostic. The FEE SECDED ECC controller utilizes the same ECC algorithm as used in the main Flash memory; 8-bit of code are implemented per 64-bit of data. Detected uncorrectable errors result in a ESM error.
In the case of a single bit error and double bit ECC error, the CPU export the error detection events to the EPC module and ESM (1.4, 2.21). I will confirm it later.