This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what are procedure steps to connect using USB port with the TDAV4M EVM board

hi,

what are procedure steps to connect using USB port with the TDAV4M EVM board.

For example the usb connection between an android mobile phone and the TDAV4M EVM board for data transfer.

thanks

Mircea

  • Hi Mircea,

    Perhaps this will help with the Wifi and Bluetooth questions as well.

    This depends on which Operating System is running, and which cores you wish to connect to.

    The simplest case will probably be when you are running Linux. You can connect to a USB device similar to how you would connect to any other Linux machine, and use Linux applications or commands to communicate with the USB device.

    Regards,

    Erick