If I want to write a program that communicates with USB, do I need to use the following pin numbers?
・ T6
・ U5
・ V4
・ W4
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If I want to write a program that communicates with USB, do I need to use the following pin numbers?
・ T6
・ U5
・ V4
・ W4
Hello Kanematu-san,
None of those pins are associated with the USB peripheral so you do not need them for such an application.
Best Regards,
Ralph Jacobi
Thank you for your reply.
If I write a program, which signal should be connected to which pin?