Part Number: LAUNCHXL2-570LC43
Other Parts Discussed in Thread: TMDX570LC43HDK
I have the TMS570LC43X development KIT and Segger JLINK Plus debugger which is compatible with this board. I want to use the JTAG connector provided on the board and debug the MCU using segger Debugger. I also have the interface board from segger to connect JLINK to TMS570 Dev Kit. I have the correct Voltages but am receiving the following error as shown in the attachment below. I will contact Segger as well regarding this issue. Is there any support that could be provided from TI, maybe from previous similar experience on what I could do or try. For now I have hit a dead end and any help would be highly appreciated.
Looking forward to your reply,
Regards,
Aadithya
SEGGER J-Link Commander V7.58c (Compiled Nov 24 2021 17:26:11) DLL version V7.58c, compiled Nov 24 2021 17:24:54 Connecting to J-Link via USB...O.K. Firmware: J-Link V11 compiled Dec 9 2021 14:14:49 Hardware version: V11.00 S/N: 601013786 License(s): RDI, FlashBP, FlashDL, JFlash, GDB VTref=2.342V Type "connect" to establish a target connection, '?' for help J-Link>connect Please specify device / core. <Default>: TMS570LC4357 Type '?' for selection dialog Device> Please specify target interface: J) JTAG (Default) S) SWD T) cJTAG TIF>J Device position in JTAG chain (IRPre,DRPre) <Default>: -1,-1 => Auto-detect JTAGConf> Specify target interface speed [kHz]. <Default>: 4000 kHz Speed>400 Device "TMS570LC4357" selected. Connecting to target via JTAG InitTarget() start Executing InitTarget() Could not measure total IR len. TDO is constant high. Can not find ICE-Pick (IRLen mismatch). Expected 0x00000006, found: 0x00000280 J-Link script: ICEPick found, enabling Cortex-R5 core. Could not measure total IR len. TDO is constant high. Can not find ICE-Pick (IDCODE mismatch). Expected 0x0000002F, found: 0x00000000 Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Can not find DAP (IDCODE mismatch) InitTarget() end RESET (pin 15) high, but should be low. Please check target hardware. InitTarget() start Executing InitTarget() Could not measure total IR len. TDO is constant high. Can not find ICE-Pick (IRLen mismatch). Expected 0x00000006, found: 0x00000280 J-Link script: ICEPick found, enabling Cortex-R5 core. Could not measure total IR len. TDO is constant high. Can not find ICE-Pick (IDCODE mismatch). Expected 0x0000002F, found: 0xA0002108 Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Can not find DAP (IDCODE mismatch) InitTarget() end InitTarget() start Executing InitTarget() Could not measure total IR len. TDO is constant high. Can not find ICE-Pick (IRLen mismatch). Expected 0x00000006, found: 0x00000280 J-Link script: ICEPick found, enabling Cortex-R5 core. Could not measure total IR len. TDO is constant high. Can not find ICE-Pick (IDCODE mismatch). Expected 0x0000002F, found: 0xA0002108 Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Can not find DAP (IDCODE mismatch) InitTarget() end RESET (pin 15) high, but should be low. Please check target hardware. InitTarget() start Executing InitTarget() Could not measure total IR len. TDO is constant high. Can not find ICE-Pick (IRLen mismatch). Expected 0x00000006, found: 0x00000280 J-Link script: ICEPick found, enabling Cortex-R5 core. Could not measure total IR len. TDO is constant high. Can not find ICE-Pick (IDCODE mismatch). Expected 0x0000002F, found: 0xA0002108 Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Could not measure total IR len. TDO is constant high. Can not find DAP (IDCODE mismatch) InitTarget() end Cannot connect to target. J-Link>