Part Number: RM46L852
Running HALCorGen version 04.07.01. Does not appear to render correctly on some of the tabs. For example ESM Channel 0-31 enable/disables do not line up with the channel text. Also there appear to be enable/disable blocks that are below the correct enable/disables. Som of the LT_Counter components are partially obscured by the enabling high/low level. Have run on both linux and windows with the same basic result. The ESM page is reasonably involved.... but it is the area that I need to configure.
bb