Other Parts Discussed in Thread: AM2632, SYSCONFIG
Team,
Customer is trying to enable both GPMC0 (Pseudo-SRAM) and ETH in the pinmux tool.
Unfortunately there are not much valid configuration available.
-Can you please help with the below?
-Could you share a config example using the cloud pinmux (https://dev.ti.com/sysconfig/#/start)?
If I use the interface GPMC0, I have a direct collision of outputs with the MII interface, regardless of whether MII1 or MII2.
Used I/O GPMC0:

MII interface:

With the MII2 interface, I even have more than the marked pins as collision.
I currently cannot find a way to use these two interfaces (GPMC & MII).
May I ask you for support?
Thanks in advance,
A