Part Number: TMS570LS1114
1. In the code provided by the diagnostic library, the Flash diagnostic code cannot be placed in the Flash address and the address specified by Sram. However, in the diagnostic library code, when module type 1114 (12X series), the code placed in Sram is shielded. Is this code wrong?

2. When the module is working for about 20 hours, there will be Flash 1 bit ECC error, and it is on different address, may I ask what is the possible cause?
Each time a fault occurs, the address is different. What is the possible cause of this phenomenon?
The address of the fault:
0x0003 76E8h
0x0003 7168h
0x0003 54F0h
0x0003 35C8h
0x0003 2210h
0x0003 2018h
0x0002 F618h
0x0002 EBC0h
0x0002 2FB0h
0x0001 3A60h
0x0001 27D8h