Part Number: TMS570LS1227
Hi,
This is regarding the use of the EEPROM Flash Bank to store configuration and other data. Based on my understanding, the TI FEE driver writes data sequentially into memory. Would it be possible to use the driver for FEE operations if the requirement is to partition the memory into sections to store different types of data?
For e.g. the first 32 bytes store system information, the next 256 bytes store configuration data, the next 1 KB stores some other data, etc. If my configuration data is 32 bytes in length, the first configuration should be stored at address 0x20. If the configuration is modified, it should be stored at the next address 0x40, and so on. When the end of the section (Address 0x120) is reached, the first record (at 0x20) should be erased and written with the new configuration. This should apply for all the partitions created in the FEE even when write calls to other sections occur between configuration writes. If this is possible, can you please elaborate on how it can be achieved?
Thanks and Regards,
Vimal