Hi Expert,
Could you let me know whether or not we can use both KUNBUS stack for EIP and Lwip stack for general TCP/IP (eg. for applications using tftp, http) in parallel?
I would like you to revisit the link below and update your current status.
FYI, when I tried to simply link Lwip library into the example of KUNBUS EIP in SDK 08.02.00.31, there were lots of the "redefined Lwip function" errors during compilation, which means the KUMBUS EIP library has already included a part of Lwip core. I think if KUNBUS EIP had linked Lwip library externally as one application using Lwip, other applications could have used Lwip core stack without any problem. I was wondering the reason why they included a part of Lwip core inside of their library. Please correct me if my idea is wrong.
I would appreciate it if you share a plan of SDK including this feature Or your experience and knowledge about how to enable/use both at the same time with the current SDK version.
Regards,
Moonil