Part Number: RM46L852
Other Parts Discussed in Thread: INA237, , SYSCONFIG
Dear Champs,
My customer connected INA237 to RM46L852 through I2C, but failed to communicate with INA237.
As there is no implementation for I2C communication in below sysconfig generated driver code,
https://dev.ti.com/sysconfig/index.html?product=ascstudio&module=/ti/sensors/currentsensor/INA237
they implemented it by themselves, but failed to communcate with INA237.
Could you please check below code or share the example for I2C communication with INA237?
~~~~~~~
uint8_t i2c_send(uint32 length, uint8 * data, uint8_t slave_Address)
{
uint8_t err_ret = 0;
// while(i2cIsTxReady(i2cREG1) == 0){}
uint16_t cnt = 0;
i2cSetSlaveAdd(i2cREG1, slave_Address);
i2cSetDirection(i2cREG1,I2C_TRANSMITTER);
i2cSetCount(i2cREG1, length);
i2cSetMode(i2cREG1, I2C_MASTER);
i2cSetStop(i2cREG1);
i2cSetStart(i2cREG1);
i2cSend(i2cREG1, length, data);
//i2cSetStop(i2cREG1);
while(i2cIsBusBusy(i2cREG1) == true){
cnt++;
if(cnt > 0x7ff){
//printf("i2c_send timeout!!\n");
err_ret = 1;
break;
}
}
cnt = 0;
while(i2cIsStopDetected(i2cREG1) == 0){
cnt++;
if(cnt > 0x7ff){
//printf("i2c_send timeout!!\n");
err_ret = 1;
break;
}
}
i2cClearSCD(i2cREG1);
cnt = 0;
while(i2cIsMasterReady(i2cREG1) == 0){
cnt++;
if(cnt > 0x7ff){
//printf("i2c_send timeout!!\n");
err_ret = 1;
break;
}
}
if (err_ret == 1) {
//printf("err_ret %d : do i2cInit\n", err_ret);
i2c_reinit();
}
return err_ret;
}
uint8_t i2c_receive(uint8 * data, uint8_t cnt, uint8_t slave_Address)
{
uint8_t err_ret = 0;
uint16_t failcnt = 0;
// uint8_t i;
// uint8_t tempData[40];
// while(i2cIsRxReady(i2cREG1) == 0){}
i2cSetSlaveAdd(i2cREG1, slave_Address);
i2cSetDirection(i2cREG1,I2C_RECEIVER);
i2cSetCount(i2cREG1, cnt);
i2cSetMode(i2cREG1, I2C_MASTER);
i2cSetStop(i2cREG1);
i2cSetStart(i2cREG1);
#if 0
i2cReceive(i2cREG1,40,tempData);
#else
i2cReceive(i2cREG1,cnt,&data[0]);
/*
if(data[0]<3)
{
i2cREG1->MDR |= 0x8000;
i2cSetStop(i2cREG1);
i2cReceive(i2cREG1,1,&data[1]);
}
else
{
i2cReceive(i2cREG1,data[0]-2,&data[1]);
i2cREG1->MDR |= 0x8000;
i2cSetStop(i2cREG1);
i2cReceive(i2cREG1,1,&data[data[0]-1]);
}
*/
#endif
//i2cSetStop(i2cREG1);
while(i2cIsBusBusy(i2cREG1) == true){
failcnt++;
if(failcnt > 0x7ff){
//printf("i2c_receive timeout!!\n");
err_ret = 1;
break;
}
}
failcnt = 0;
while(i2cIsStopDetected(i2cREG1) == 0){
failcnt++;
if(failcnt > 0x7ff){
//printf("i2c_receive timeout!!\n");
err_ret = 1;
break;
}
}
failcnt = 0;
i2cClearSCD(i2cREG1);
while(i2cIsMasterReady(i2cREG1) == 0){
failcnt++;
if(failcnt > 0x7ff){
//printf("i2c_receive timeout!!\n");
err_ret = 1;
break;
}
}
i2c_delay(100);
// memcpy(data,tempData,tempData[0]);
return err_ret;
}
int8_t mcu_i2cTransfer( uint8_t busId, uint8_t i2cAddr,
uint8_t *dataToWrite, uint8_t writeLength,
uint8_t *dataToRead, uint8_t readLength)
{
/*
* Add MCU specific I2C read/write code here.
*/
int8_t err_ret = 0;
err_ret = (int8_t)i2c_send(writeLength, dataToWrite, i2cAddr);
if(err_ret != 0){
printf("send err\n");
}
else if(readLength > 0){
err_ret = i2c_receive(dataToRead, readLength, i2cAddr);
if(err_ret != 0){
printf("receive err\n");
}
}
return err_ret;
/*
* Add MCU specific return code for error handling
*/
return (0);
}
~~~~~~~~
Thanks and Best Regards,
SI.