Part Number: TMS570LS3137
Hello,
I am trying to debug my application with OpenOCD, however I experience a lot of problems with this task. I am using JLink Base as my debugger, below is my OpenOCD config file:
set DAP_TAPID 0x0B8A002F set JRC_TAPID 0x0B8A002F source [find interface/jlink.cfg] transport select jtag source [find target/ti_tms570.cfg] reset_config trst_only
JFlash has no problems with connecting to the target and reading/writing flash, but OpenOCD does not allow to debug my application, here is the output:
Open On-Chip Debugger 0.11.0+dev-00571-g254883597 (2022-02-17-13:22) Licensed under GNU GPL v2 For bug reports, read http://openocd.org/doc/doxygen/bugs.html Info : TI BE-32 quirks mode is enabled trst_only separate trst_push_pull Info : J-Link V10 compiled Nov 2 2021 12:14:50 Info : Hardware version: 10.10 Info : VTarget = 3.328 V Info : clock speed 1500 kHz Info : JTAG tap: tms570.jrc tap/device found: 0x4b8a002f (mfg: 0x017 (Texas Instruments), part: 0xb8a0, ver: 0x4) Info : JTAG tap: tms570.cpu enabled Warn : Debug base address for target tms570.cpu has bit 31 set to 0. Access to debug registers will likely fail! Please fix the target configuration. Info : tms570.cpu: hardware has 6 breakpoints, 2 watchpoints Info : starting gdb server for tms570.cpu on 3333 Info : Listening on port 3333 for gdb connections Info : JTAG tap: tms570.jrc tap/device found: 0x4b8a002f (mfg: 0x017 (Texas Instruments), part: 0xb8a0, ver: 0x4) Info : JTAG tap: tms570.cpu enabled Warn : Debug base address for target tms570.cpu has bit 31 set to 0. Access to debug registers will likely fail! Please fix the target configuration. Warn : tms570.cpu: ran after reset and before halt ... Error: timed out while waiting for target halted TARGET: tms570.cpu - Not halted GDB Server stopped, exit code 1
Do you have an idea how to config OpenOCD to be able to debug TMS570 application?
Regards,
Bartek