Part Number: SIMPLELINK-MSP432-SDK
Hi Folks,
I am using MSP432P401R with FreeRTOS. When I configure the GPIO to handle the interrupt, the I2C read failure happens on I2C slave device after 30 hours since boot.
Way to configure the GPIO interrupt:
GPIO_setConfig(Board_GPIO_BUTTON0, GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_FALLING);
/* install Button callback */
GPIO_setCallback(Board_GPIO_BUTTON0, gpioButtonFxn0);
/* Enable interrupts */
GPIO_enableInt(Board_GPIO_BUTTON0);
Is there any reason that GPIO interrupt configuration can cause this kind of failure?
Regards,
Amit