Part Number: TMS570LC4357
Hi experts,
In the Technical Reference Manual Chapter 2.5.3.30 is a description of how the Quadrants are represented in the PS0 to PS31 registers. It is stated that the description is only viable for PS0 to PS31.
However there is no similiar description concerning the other registers, e.g. PPSE0MSTID_L. The beahviour of PPSE0MSTID_L that we observed would suggest that the description is also viable for these registers ( For PPSE0MSTID_L/H only Quad0 is implemented and the slave connected there is using only 2 Quads)
(Q1) Is the description in chapter 2.5.3.30 also viable for PPSExMSTID and PPSxMSTID Registers?
Thank you and best regards,
Max