Part Number: TMS570LS1115
Hi team,
Here's an issue from the customer may need your help:
During bench test, there is no problem with the small torque. High torque has the following error:
CAN communication is lost, supply current is reduced, ePWM output frequency is changed to 1k (designed to 10K).
The single-board simulation found that the behavior was similar to the one above when the crystal was shorted. The customer would like to know if the TMS570LS1115 have an internal crystal and which pin is powered by the signal pin corresponding to the external crystal oscillator.
Could you help check this case? Thanks.
Best Regards,
Cherry