Part Number: EK-TM4C123GXL
I do not make it to redirect the usb-serial to another uart than uart0.
In usb_dev_serial i changed the uart defines to match uart1:
#define USB_UART_BASE UART1_BASE
#define USB_UART_PERIPH SYSCTL_PERIPH_UART1
#define USB_UART_INT INT_UART1
#define TX_GPIO_BASE GPIO_PORTB_BASE
#define TX_GPIO_PERIPH SYSCTL_PERIPH_GPIOB
#define TX_GPIO_PIN GPIO_PIN_1
#define RX_GPIO_BASE GPIO_PORTB_BASE
#define RX_GPIO_PERIPH SYSCTL_PERIPH_GPIOB
#define RX_GPIO_PIN GPIO_PIN_0
In startup_ccs.c i changed:
void (* const g_pfnVectors[])(void) = {
....
IntDefaultHandler // UART0 Rx and Tx
USBUARTIntHandler, // UART1 Rx and Tx
...}
What am i missing?