This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM46L852: RM46L852 MibSPI buffers relation to CPU memory

Part Number: RM46L852
Other Parts Discussed in Thread: ADS1258

Dear Support, 

We implemented electronic boards housing a RM46L852 and two Analog Devices AD7124 ADCs.

The ADCs are separately and exclusively connected to MibSpi Ports (MibSpi3, MibSpi5) of the RM46 running a safety OS.

We run the ADCs in the single conversion mode, while each ADC is configure to automatically run a sequences of 9 different

conversions.  

Similar to the TI ADS1258 these ADCs buffer only one conversion result of a sequence, forcing the µC to read each conversion

after a finished conversion. The AD7124 does not have a separate pin for indicating a finished conversion  (not_RDY like the TI

ADS1258 ), but does it by pulling down the data output line (DOUT). Therefore we connected the ADCs DOUT lines to GIO pins

of the RM46. After each start of conversion these GIOs are sensed as low trigger CPU interrupt. While such an interrupt starts the

readout out the dedicated ADC Channel Data via its related MibSPI port in master mode.  

Thus all parameterization, control and readout of the ADCs is actually controlled by the CPU, though we know, that such things are

better done by DMA access.

So far this way is choosen to avoid any interferences with our safety related test of the CPU Memory additionally running.

 

Now for time critical sensor implementations we run into an unacceptable high CPU load caused by this kind of ADC driver.

Therefore we need to find a solutions and like to check the possibility of using MibSPI transfer groups.

Our Datasheet and Technical Reference Manual inspection showed no functional obstacle for autonomously reading the mentioned

ADCs via the MibSpi transfer groups.

The read ADC Buffers on each MibSpi are:

  • 9 x 8 Bit command register
  • 9 x 8 Bit status register
  • 9 x 24 Bit data register
  • 9 x 24 Bit error register

Which sums up to 576 Bit, or 72 Byte.

We like to know, if TI agrees with our idea of reading this ADCs conversion sequences via transfer groups?

Additionally it would be helpful to receive some advice, guidance or even examples for such an implementation, if possible?

A further question results from the fact, that the DOUT line is identical to the not_RDY line for the chosen ADCs.

It means, since prior or further transmissions on the same MibSpi port always include DOUT/not_RDY low levels, the trigger of

the groups needs to be enable/disable between each conversion data reading. As I found, this is possible by doing it like the

midspiSetfunctional()method of mibspi.c is doing, isn’t it?

 

By reading the Technical Reference Manual and the Datasheet we found mismatching explanations about the interaction of transfer

groups with memory.

The Datasheet says, that each MibSPI port has a dedicated memory providing 128 buffers to the transfer groups. By this we assume,

that the MibSPI periphery has a separate memory independent or at least somehow hardware separated from the CPU memory.

On the other hand the Technical Manual talks about DMA accesses. These may induce intercations of transfere groups or accumulated

data on the same memory range as the CPU. Therefore our safety related tests on the CPU memory may detect a lot of errors due to

hardwares direct accesses on the CPU memory (CPU RAM DMA).

The Technical Manual claims DMA as an option and a separate hardware of 128 buffers is described in the Datasheet and the

Technical Manual. Thus my impression is, that these bufferes are exactly invented to overcome such safety issues, isn't it? 

Therefore we need to ask, if someone from TI Side can give us a definitiv statement about a hardware base separation of the 128 MibSPI

buffers from the CPU memory?

Otherwise it seems like we are not willing to take the risk.   

  • 128 MibSPI

    buffers from the CPU memory?

    The MibSPI RAM is a different memory space from the CPU memory. The CPU SRAM is from 0x08000000 to 0x0802FFFF, and MibSPI RAM is from 0xFF0A0000 to 0xFF0F0000 (MibSPI5,3,1). 

    If the ADC device generates a trigger after each data conversion, you can use SPI compatible mode, and use DMA to transfer the received data from SPIBUF to CPU memory.

    If the ADC device generate a trigger after the conversion of a group of data, it's good to use transfer group, and use the DMA to transfer data from TG to CPU memory.

  • It seems like CPU und MibSPI use the RAM but different address spaces. Does it mean, that running memory test from the TI safety library on the CPU memory won't interfere and cause false memory errors, during MibSPI is is operating on its dedicated RAM space?  

    As I understand, your advice is to is to use DMA on the CPU memory range in case of our choosen ADC? In case memory test won't interfere with the MibSPi memory space, is DMA on this memory space possible as well?  Because years ago we requested to TI, if DMA on the CPU memory can interfere with running safety library memory tests and the result was no definitiv or sufficient statement!

    Our suggestion to avoid DMA was to use the transfer groups to collect the ADC data by activating the tigger functionality of a certain transfer group after an acquisition request and to deactivate it at the end of collection. Of course this somehow forces an automatic incrementation of the RX buffer during the data collection. Does this work? Or does a next trigger always overwrite the previous data, since the data is only collected to the RX register of the triggered transfer group buffer holding the TX?

    If so, in case multiple transfer groups are defined with the same trigger event and buffer size, are all of them executed simultaniously by an arising trigger, or sequential, first trigger frist group, second trigger second group, and so on?   

  • Hi Mike,

    I am sorry for coming back late. Have you resolved your issue?